EVSOLCG001EN-01

Importing EcoStruxure EV Charging Expert Configuration

If you want to restore or re-use a saved configuration, you can select Import Configuration when opening EcoStruxure EV Charging Expert.

A pop-up window allows you to recover a configuration from a previous configuration export.

NOTE: The configuration file with version 6.0.0 or higher is compatible. It requires configuration file password to be installed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?