EVSOLCG001EN-01

Updating EcoStruxure EV Charging Expert Firmware

Select the hamburger menu and Device Update.

The following screen is displayed while the new version is being installed.

It takes about one minute to run the firmware installation. After one minute, EcoStruxure EV Charging Expert reboots, with the up-to-date firmware version.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?