EVSOLCG001EN-01

Key Variables

The commissioning of the EV infrastructure depends on the following key variables:

  • Ranges and models of charging station: AC and/or DC charging stations

  • EV load management system:

    • Installation of EcoStruxure™ EV Charging Expert

    • Definition of the load management mode (static or dynamic)

  • Operational requirements:

    • Local operation only

    • Connection to a remote charging station management system (Schneider Electric or third party)

  • IT/Network configuration

    • With or without DHCP server from customer site

    • Internet connectivity and network topologies (star, daisy chain, or ring)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?