EVSOLCG001EN-01

Relaunching the Discovery Process

When all the charging station firmware are updated to the latest version:

  1. Restart EcoStruxure EV Charging Expert wizard.

  2. Re-launch the discovery process.

    The firmware versions are up to date and all charging stations are discovered.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?