EVSOLCG001EN-01

Configuring Power Meters

Configure power meters if you have dynamic or local energy production zones on the EV infrastructure.

NOTE: To monitor the local energy production, the power meter wiring must include a neutral and be wired in the correct direction.

In case of several photovoltaic production zones, one power meter per zone is required.

For more information about static and dynamic zones, refer to the video showing how to configure load management parameters:
https://youtu.be/c3FBqzF1Avw

For more information about power meter configuration (reconfiguration or customization), refer to Charging Stations Commissioning in DOCA0358EN EcoStruxure EV Charging Expert User Guide.

Link one power meter to each dynamic zone as follows:

  1. From the Power Meter menu, select the + sign.

  2. To define a pre-configured power meter, select Define Power Meter Models.

    NOTE: If you already have pre-configured power meters, go directly to the following step.

  3. Select Manage Power Meters.

  4. Select a power meter from the list of proposed models.

  5. To configure the power meter, fill in the following fields:

    • Name

    • Model

    • IP Address

    • ID Port

    • Slave ID or Name model RTU slaveID if RTU device.

  6. Select Save.

  7. Select Next.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?