EVSOLCG001EN-01

Saving and Exporting Configuration

It is recommended to save a backup of the current system configuration and import it later to restore a lost configuration.

The configuration export contains the following information:

  • Administrator and user profiles credentials

  • Charging stations configuration

  • Zones configuration

  • Power meters configuration

  • Network configuration

  • Authentication strategies

  • List of RFID cards

  • Authentication groups

To save a backup of the current system configuration:

  1. Select ADMIN > Save.

  2. To generate the backup file, enter a password and confirm the password.

  3. Save the exported file in a relevant repository.

    NOTE: To help ensure the security of your information, the exported file is encrypted and signed.

  4. To check that your EV infrastructure is commissioned and operational, check the following:

    • All charging stations are connected and connectors are available.

    • Use an EV charging simulator to check that the charge works well.

    • Digital inputs are operational by testing them manually.

    • Time of use is confirmed during operation.

    • Data flow is available on your EcoStruxure EV Charging Expert monitoring dashboard.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?