EVSOLCG001EN-01

Configuring the PC to Connect to EcoStruxure EV Charging Expert

  1. Connect your PC to the EcoStruxure EV Charging Expert Ethernet network.

  2. Open the local network properties menu on your PC.

  3. Open the Internet protocol TCP/IP v4 properties.

  4. Set the static IP address properties as follows:

    • IP address: 192.168.0.x (where x is a number between 50 and 100)

    • Subnet mask: 255.255.255.0

    • No default gateway

    • No DNS server

    • No proxy

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?