EVSOLCG001EN-01

Updating the Charging Station Settings

For the group of charging stations discovered (up to 10), check or update if necessary the following fields.

Fields to be updated

Charging station name

Selection of DHCP versus fixed IP address (for EVlink Pro AC only)

Phase rotation per connector (for all AC charging stations)

Box ID

VIP charging mode

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?