EVSOLCG001EN-01

Setting up the Ring Network

  1. Closing the loop

    1. Close the network loop by connecting both ends of the existing daisy chain to two ports on the managed switch.

    2. Check that the managed switch is still connected to the LAN network and/or the EV Charging Expert.

      For example, on a Schneider Electric Modicon managed switch, the connection should look like on the following picture.

  2. Check that the ring topology is working correctly:

    • All EVlink Pro AC charging stations are operational (green LED).

    • All EVlink Pro AC charging stations are connected to EV Charging Expert and/or the charging operator (CPO) and are available in the remote management interface.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?