EVSOLCG001EN-01

Description of System Architectures

The five system architectures are the following:

  • System Architecture 1: Full architecture: supervision - edge load management - charging stations. IT including DHCP server is managed by the customer.

  • System Architecture 2: No supervision. Edge load management and charging stations operated locally by the customer.

  • System Architecture 3: With supervision - charging stations. No edge load management. A 4G cellular modem as an internet gateway and DHCP server.

  • System Architecture 4: Full architecture: supervision - edge load management - charging stations. A 4G cellular modem as an internet gateway and DHCP server .

  • System Architecture 5: Full architecture: supervision - edge load management - charging stations. A 4G cellular modem as an internet gateway limited to the connection to the supervision, and without DHCP server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.