EVSOLCG001EN-01

Offers and Commissioning Tools

Schneider Electric offers and commissioning tools are as follows:

EcoStruxure EV Charging Expert

HMIBSCEA53D1E•• licenses

HMIBX1A0NEVB100SCP license

EcoStruxure EV Charging Expert 6 is a load management system that helps control EV infrastructure and distribute available power to the charging stations.

It allows EV charging to be monitored, controlled, and maximized based on the real-time available power in the building.

It helps to ensure the respect of cost and energy efficiency constraints of a set of charging stations by controlling their operation. The controller runs its management program according to the selected parameters and data received from the charging stations.

The main functions performed by EcoStruxure EV Charging Expert charging load management system are the following:

For more information, refer to:

Schneider Electric Energy and Building Management Systems

EV load can be integrated into a facility management system, with the following features:

  • All-in-one monitoring of the electrical distribution:

    • A single interface to supervise and monitor the EV charging infrastructure integrated into the building electrical distribution network

    • Detailed alarms to make quick and informed decisions if something happens

    • Detailed view of circuit capacity to optimize the electrical distribution and to forecast EV infrastructure evolution

  • Power demand and power quality monitoring:

    • EV charging station status and usage continuous monitoring

    • Monitoring and EV charging stations power output to control the peak demand

    • Power quality view to analyze the impact of DC charging on the electrical distribution network and anticipate adverse effects

  • Energy consumption trends and KPIs:

    • Identification of the charging stations with the highest consumption

    • Consumption comparison per zone, time period, or parking usage

  • EcoStruxure Building Operation software

EcoStruxure Building Operation is a building management software that delivers the right information when, where and how you want it. Operations are simplified with drag-and-drop trending, calendar-like schedules and one-click reporting. Native open protocols provide the freedom to choose the right equipment for your application. EcoStruxure Building Operation software provides up to 30 % energy savings. It helps create a healthy and sustainable environment.

For more information, refer to www.se.com.

eSetup Commissioning Application for Electricians

eSetup is a dedicated application to configure and commission Schneider Electric products. It can be used to commission EVlink Pro AC and Schneider Charge Pro charging stations manually.

Download eSetup:

  • From Apple Store:

  • From Google Play:

  • Via your mySchneider account

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.