EVSOLCG001EN-01

Managing Basic Authentication and Charge Point Operator Certificates

Managing Basic Authentication

To help secure communication between EcoStruxure EV Charging Expert and supervision, add a basic authentication password for all charging stations. There are two options:

  • One unique password for each charging station:

    1. Select each charging station on the installation page.

    2. Select Change password.

  • Same password for all charging stations: when this option is selected, a popup appears to add a basic authentication key according to two formats (ASCII or HEXA format). The password is used for all charging stations. It can be changed later by supervision through OCPP commands.

Managing Charge Point Operator Supervision Certificates

To manage charge point operator supervision certificates:

  1. Select ADMIN > Certificates.

  2. To add or delete certificates, select Manage Certificates. For example, you can upload in this bank of certificates a new remote supervision certificate to perform a WebSocket secure connection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?