EVSOLCG001EN-01

Setting Up a Ring Topology for EVlink Pro AC Range

This chapter provides you with information about the commissioning of a ring topology cable network for EVlink Pro AC charging stations. It contains generic information for configuring the switch in your installation, as well as examples based on a Modicon switch.

This chapter explains how to:

  • Update the EVlink Pro AC charging station and activate the RSTP protocol using eSetup

    .
  • Install the switch configuration software on your PC.

  • Configure the Modicon switch used to form a ring topology. For more information refer to Configuring the Switch.

For more information, refer to:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?