EVSOLCG001EN-01

Creating an Installer Account

The Credentials screen is the following.

Create an administrator profile and a user profile:

  • Administrator: has access to all configuration for EcoStruxure EV Charging Expert and needs to complete the initial configuration before users can access the interface.

  • Users: after initial configuration, users can monitor the installation status, and manage badges.

Fill in the following fields:

  • Username: do not use Root, Admin or Administrator, as they are easy to guess.

  • Password: the password must satisfy the required conditions.

  • Check box to indicate that you securely stored these credentials. A factory reset is the only option if they get lost.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?