EVSOLCG001EN-01

Configuring the 4G Cellular Modem with DHCP

Prerequisites

Before starting the configuration of the EVP3MM 4G cellular modem:

  1. Locate the SIM card slot marked SIM on the side of the 4G cellular modem.

  2. Push the SIM card into the slot until it snaps into place.

  3. Connect to the network according to the IT connectivity map.

  4. Open a web browser.

  5. Type https://192.168.0.254/ in the URL field.

  6. Select the Advanced button to authorize the non-secure connection.

  7. Select Proceed to 192.168.0.254.

  8. On the login page, enter the following:

    • Username: admin

    • Password: EVlink4EV!

Configuration Procedure

Download the latest firmware of your device from the factory website.

To configure the 4G cellular modem:

  1. In the left panel, select Administration > Firmware Upgrade.

  2. Browse the downloaded binary and select it.

  3. Select Start Upgrade.

    Upgrade can take up to 10 minutes. When upgrade is complete, the modem reboots automatically.

  4. Check on the following screen that the cellular radio firmware is updated.

  5. In the left panel, select Cellular > Cellular Configuration.

  6. In General Configuration, set the Mode to PPP.

  7. In Modem Configuration, from Cellular > Cellular Configuration > Modem Configuration, set the APN to mbb.mobi-data.com.

  8. In Authentication, from Cellular > Cellular Configuration > Authentication, set the Authentication Type to NONE.

  9. Select the Submit button at the bottom left of the screen.

  10. In the left panel, select Save and Apply.

  11. Select OK to apply the changes. The 4G cellular modem reboots.

Checking the Configuration

To check the configuration of the 4G cellular modem:

  1. On the Home page, in the WAN section, check that the State is the following: PPP Link is up.

  2. Check that the CD green LED on the 4G cellular modem is on.

  3. Check that DHCP server is set up according to the customer IT inputs (in the correct address ranges) in EcoStruxure EV Charging Expert.

  4. Check the internet connectivity.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?