EVSOLCG001EN-01

Connecting to EcoStruxure EV Charging Expert

  1. Open a web browser.

  2. Type 192.168.0.128 in the URL field.

NOTE: A message may be displayed. If this occurs:
  1. Select the Advanced button to authorize the non-secure connection.

  2. Select Proceed to 192.168.0.128 (unsafe).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?