EVSOLCG001EN-01

Finishing the Installation of the Selected Charging Stations

To finish the installation of the selected charging stations:

  1. Select the charging station(s) for which you want to finish the installation.

  2. Select Install Selected.

  3. On the pop-up window; select Close.

    EcoStruxure EV Charging Expert installs the charging stations in the system.

    All the charging stations reboot to finalize their installation in EcoStruxure EV Charging Expert.

  4. Repeat step 14 to step 17 for Architecture 1 for each group of 10 charging stations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?