EVSOLCG001EN-01

Configuring the 4G Cellular Modem without DHCP

If you do not need the DHCP server, you can disable the 4G cellular modem as a DHCP server.

Prerequisites

Before starting the configuration of the EVP3MM 4G cellular modem:

  1. Locate the SIM card slot marked SIM on the side of the 4G cellular modem.

  2. Push the SIM card into the slot until it snaps into place.

  3. Connect to the network according to the IT connectivity map.

  4. Open a web browser.

  5. Type https://192.168.0.254/ in the URL field.

  6. Select the Advanced button.

  7. Select Proceed to 192.168.0.254.

  8. On the login page, enter the following:

    • Username: admin

    • Password: EVlink4EV!

Configuration Procedure

To configure the 4G cellular modem:

  1. In the left panel, select Setup.

  2. Select the DHCP Configuration tab.

  3. In the displayed list, identify the DHCP server used.

  4. In the Options column, select the pen to edit the parameters.

  5. Deselect the Enabled check box.

    On the Home screen, the DHCP State indicates Disabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?