EVSOLCG001EN-01

EcoStruxure EV Charging Expert User Interface

EcoStruxure EV Charging Expert monitoring dashboard displays the following information:

  • Ongoing status of all the charge points (connectors)

  • Load transaction

  • Zone configuration

Monitoring dashboard also allows you to manage charging stations:
  • Reboot the charging stations

  • Start and stop remotely a charging station

  • Publish a diagnostic report

Monitoring dashboard is the following screen.

Monitoring dashboard

  1. Zone panel

  2. Export Transactions button

  3. Dashboard giving information about zones and charging stations

  4. Transaction information and management

  5. Charging stations assignment and management

Zone Screen

When you select a zone in the zone panel, the following zone screen is displayed.

  1. Station Fleet: status of the charging stations assigned to the selected zone

  2. Current Repartition describes the charging setpoint available according to the active zone maximum current, zone consumption and transactions information:

    • Allocated: allocated current to charging stations during transaction

    • Reserved: reserved current for building consumptions and disconnected stations (degraded setpoint applies to charging station).

    • Grid: available current from grid (with reduction)

    • Local: available current from local production

    • Extra Setpoint: reallocated setpoint from suspended transactions

Transaction Information and Management

The following transaction information is displayed.

  1. ID: unique identifier of the transaction

  2. Station: station name and connector used for the charging session

  3. RFID Card: RFID card which launches the transaction

  4. Status: status of the transaction according to OCPP standard:

    • Charging

    • Suspended by Vehicle

    • Suspended by System

    • Finishing

    • Available

    • Preparing

    • Faulted

    • Unavailable

    • Unknown

  5. Phase: phases selected by EV (mono-phase or tri-phased)

  6. Date/Duration: transaction start date and effective charging duration (time spent in charging state)

  7. Energy: energy consumed by the ongoing transaction

  8. Setpoint: current setpoint (current intensity or power allocated to the ongoing transaction)

  9. Consumption: actual consumption of the vehicle (current or power)

Station Screen

When you select a charging station in the zone panel, the station screen provides the following information.

  • Name

  • Charge box identity: used for remote supervision

  • VIP status: option to enable VIP access to the charging station

  • Electrical phase configuration of the charging station

  • Vendor of the charging station

  • Firmware version and management

  • Current allocated to the charging station in degraded mode

In the station screen, the following log section displays all OCPP commands received by EcoStruxure EV Charging Expert from the selected charging station.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?