EVSOLCG001EN-01

System Architecture 4: Presentation

The main characteristics of system architecture 4 are the following:

  • EcoStruxure EV Charging Expert is not used

  • DHCP server hosted by 4G cellular modem, internet connectivity provided via the SIM card supplied by the charge point operator

  • Digital network: star or daisy chain using managed switches

  • EV infrastructure operated by an external charging point operator

  • Greenfield architecture

System architecture 4 can be implemented for the following models of charging stations:

Charging station Minimum version

Schneider Charge Pro

1.18.1

EVlink Pro AC

1.3.8

NOTE: For DC fast charging station and for Schneider Electric legacy ranges of charging stations, contact your local front office.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?