Creating Zones and Sub-Zones
You can create a maximum of 20 zones and four levels of sub-zones in each zone.
A zone can include charging stations and energy production.
In case of several photovoltaic production zones, one power meter per zone is required.
-
To create a zone from Zones menu, select the + sign.
-
For each created zone, fill in the following fields depending on your Energy Management Directive (Dynamic / Static):
-
Name
-
Maximum Current
-
Degraded Mode Zone Setpoint
-
Associated Power Meter, if any
-
Maximum Current of a static zone
-
Degraded Mode Zone Setpoint of a dynamic zone
For a dynamic zone, a Degraded Mode Zone Setpoint defines the maximum current always available for EV charging, irrespective of other load in the same electrical zone. Enter a value for Degraded Mode Zone Setpoint that allows you to manage charging stations even if EcoStruxure EV Charging Expert loses building consumption information.
For a dynamic zone, offline management is active when communication is lost with the charging station or with the power meter dedicated to this zone.
-
-
To create a sub-zone in a zone, select the + sign corresponding to this zone.

-
For each created sub-zone, fill in the following fields:
-
Name
-
Maximum Current
-
-
Associate a power meter if needed. For local production, select the power meter that measures the energy produced by the photovoltaic of this zone. A power meter cannot be shared by several zones. In case of several photovoltaic production zones, one power meter per zone is required.
-
Select Save and Next.
For more information about the creation of zones and sub-zones,
refer to the video showing how to configure
loads' parameters with EcoStruxure EV Charging Expert & assign chargers to a zone:https://youtu.be/c3FBqzF1Avw