0000649744_02_en

Gutor Battery Management System (G.BMS)

The Gutor battery management system (G.BMS) is a solution that actively balances the charge of each battery block. The G.BMS continuously monitors the voltage, impedance, temperature and as an option the electrolyte level. The measured information is used to equalize the charge of the individual blocks to help them reach their designed lifetime.

Any Gutor system with a battery can use the G.BMS solution since it is installed separately from the system. The G.BMS solution can also be installed on already existing batteries.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?