0000649744_02_en

How to Start the Battery Circuit Test

Before you start the battery circuit test check:

  • That the settings for the test is correct.

  • That the battery is connected.

  • That the battery breaker is closed.

  • That the rectifier modules are in float charge.

NOTE: It is not possible to start the test with the rectifier modules in boost charge, equalizing charge or battery operation.

  1. Make sure you are logged in as a user with Service access.
  2. Press the Settings icon and navigate to Service > DC System 1 > Battery tests.
  3. Press the Start button in line with Start battery circuit test to start the test.

This test does not discharge the battery, it only checks that the battery is correctly connected to the circuit.

If the voltage stays above the set voltage level for the set time, the battery circuit test is successful.

In case the voltage drops below the set voltage level at any time, the test is interrupted and considered unsuccessful.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?