0000649744_02_en

Network Management Card (NMC) and Communication

In Gutor systems a network management card (NMC) can be used to send alarms, events and status indications over a local or remote network to a customer device for monitoring.

From the NMC the following communication options and protocols are available:

NOTE: Each communication option or protocol can be enabled/disabled and must be configured correctly before use.
  • Web interface through HTTPS and HTTP

  • Command line interface (CLI) through SSH and Telnet

  • File transfer through SCP and FTP

  • Modbus TCP/IP

  • Modbus Serial/RTU with RS-485 4-wire full duplex

  • SNMPv3 and SNMPv1

For more information about the NMC and how to configure the settings see the Network Monitoring System user guide.

The NMC can be combined with additional gateways for further protocols:

  • IEC 61850

  • Profibus DP

  • Others on request

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?