0000649744_02_en

User Accounts

To secure information and settings it is only possible to view some basic information from the display without a login.

To change settings and view more information a login is required. Depending on the access level of the user, different information and settings will be available from the display.

The different access levels are:

  • Viewer: Can only view some basic information like measurements, events, general information and settings (no login).

  • Owner: Can view a bit more information like logs. Can also modify some general information like date, time, language and site information.

  • Service: Can view and modify system settings, change operation modes and perform tests.

NOTE: A gray input field means that the information cannot be modified.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?