0000649744_02_en

How to Start the Relay Tests

During the relay test the relay switches to its active state. Before starting make sure that it is approved to perform the test, especially if the active relay signal triggers an remote action.
  1. Make sure you are logged in as a user with Service access.
  2. Press the Settings icon and navigate to Service > General > Relaytest > Relaytest.
  3. If necessary, expand the section for the input/output card to show the programmed relays.
    NOTE: For more information about the relays refer to the Drawings.
  4. Press on the Start button for the relay you want to test.
For a few seconds the relay will change to its active state for a short time (open if normally closed, closed if normally open). Check that the connected signal was correctly activated when the relay state changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?