0000649744_02_en

Rectifier Modules

The rectifier module converts AC (input) to DC (output). The module is fan cooled.

Different output voltage levels are available: 24, 48, 60, 110/125 and 220 V DC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?