0000649744_02_en

General Settings

After startup but before operation, the site information should be filled in and some basic system settings should be configured.

Press the Settings icon and navigate to Settings > General. The pages that can be accessed for here are:

  • Date and time: Set the system date, time, time zone and clock display format.

  • Language: Set the language for the system display.

  • Display: Change the display brightness and time until the display turns off after inactivity.

  • Site information: Information about the system owner’s site.

  • Data sheet: General data about the system.

NOTE: User login with Owner access level or higher is needed to change the general settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?