0000649744_02_en

Measurements in the Display

There are multiple different measurements that can be viewed in the display, and some can be accessed in multiple ways.

  • System Measured Values: Quick access to main measurements about the output.

  • System State (Modules): Detailed measurements about the modules.

  • System State (Batteries): Detailed measurements about the batteries.

  • Measured Values (Protocol): Detailed configured list of measurements about the system, modules and batteries.

System Measured Values

To view the System measured values click on Measurement icon in the Status bar at the bottom of the screen.

System State (Modules)

To view the Measured values for the rectifier it is possible to either:

  • Click on the Rectifier modules icon on the home screen.

  • Navigating to System state > DC System 1 > Rectifier/DCDC.

System State (Batteries)

To view the Measured values for the battery it is possible to either:

  • Click on the Battery icon on the home screen.

  • Navigating to System state > DC System 1 > Battery.

Measured Values (Protocol)

To view the configured list of Measured values, navigate to Protocol > Measured values.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?