0000649744_02_en

Measurements

The available measurements can be viewed from the display. As an option, additional measuring instruments can be installed in the door.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?