0000649744_02_en

Safety Precautions

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Follow safe electrical work practices. See NFPA 70E or CSA Z462, or according to your local standards and regulations.
  • Always use appropriate personal protective equipment (PPE).
  • All safety information must be read, understood and followed.
  • Only qualified personnel are allowed to install, operate and perform maintenance on the system.
  • Isolate all power supplies (including the battery) before working on or inside the system.
  • Always use a properly rated voltage sensing device to check for hazardous voltage between all terminals, including the protective earth (PE).
  • Reinstall all parts and protective covers before turning on any AC power supply or connecting a DC power source to the system.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Always wait 5 minutes after turning off the system and isolating all the power supplies (including the battery) before removing any parts or protective covers. The system contains DC capacitors with long discharge time.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The system must be connected to protective earth (PE). Always connect the system to protective earth (PE) before connecting any power supply.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Battery circuit breakers must be installed according to the specifications and requirements as defined by Schneider Electric.
  • Battery maintenance must only be performed by qualified personnel knowledgeable of batteries and the required precautions.
  • Always disconnect the charge source before you connect or disconnect the battery to the terminals.
  • Never open, alter or damage batteries. This can release toxic electrolytes that are harmful to the skin and eyes.
  • Never dispose of batteries in a fire as they can explode.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
When replacing batteries, always replace with the same type and number of batteries or battery packs.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Never drill or cut holes in or near the system.
Failure to follow these instructions will result in death or serious injury.
WARNING
Hazardous vapors
Fire inside the system can produce hazardous vapors that should not be inhaled.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
unintended Equipment operation
Never connect the system output to regenerative loads, for example, photovoltaic systems or speed drives.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
System OVERHEATING
Always be aware of the space requirements around the system for ventilation and operation.
Never cover the product’s ventilation openings when the system is in operation.
Failure to follow these instructions can result in equipment damage.
NOTE
Always recycle and dispose of any waste in accordance with local regulations and rules.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?