Display Overview
On the home screen there are multiple buttons and sections with information.
- (A) Virtual LED bar: The Virtual LED bar on the left side shows the system virtual LEDs. Up to 39 virtual LEDs can be used. Press the Double arrow icon to show more information about the LEDs and to scroll in the list of LEDs.
- (B) Header bar: Shows the logo and the current screen name. In the top right corner of the Header bar there is a Settings icon for the main menu and the User icon or the Username. If a buzzer alarm is active a Mute icon is also shown.
- (C) User icon / Username: If no one is logged in the User icon is shown. Press the User icon to login. If a user is logged in the username and access level will be displayed.
- (D) Settings icon: Press to show the main menu options. Press a menu option to navigate to the page. To hide the main menu press at the top of the bar, anywhere outside the main menu or wait 10 seconds.
- (E) Content area: Shows the information on the current page. From the Home screen the Rectifier modules icon and the Battery icon can be pressed to view additional information and measurements.
- (F) Status bar: The Status bar shows buttons for quick navigation. The buttons shown depend on the currently active menu or screen.
- (G) Measurements icon: Press to enter the System measured values page that shows voltage, current and output power measurements.
- (H) Home icon: Press to enter the Schematic screen, it shows a mimic of the system status. It is also called the Home screen since it is the first screen that is shown.
- (I) Date and time: Shows the current date and time. Press to enter the Date and time menu.