0000649744_02_en

How to Change to Direct Feed

NOTICE
Incorrect Output values
Never enable direct feed in systems with a battery.
Failure to follow these instructions can result in equipment damage.
  1. Make sure you are logged in as a user with Service access.
  2. Press the Settings icon and navigate to Service > DC System 1 > Switching operations.
  3. Press the Direct feed button.
    NOTE: The current active operation mode is indicated by the black icon.
  4. Confirm the change.
The system has changed to direct feed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?