0000649744_02_en

Message List

The system status indications and alarms are available in the message list. By default, a standard configuration of the message list is available. On request the message list can be customized.

The alarms and indications can be configured as a Hold alarm. A Hold alarm requires a manual reset to remove the active state.

It is also possible to configure activation of an internal buzzer in case the alarm or indication is active. An icon for muting the buzzer is shown in the Header bar at the top of the display if the buzzer is active. Press the Mute icon to mute the active buzzer.

Severity classification:

  • Critical: A critical alarm exists, which requires immediate action and will cause damage if it is not addressed.
  • Warning: An alarm condition requires attention and could cause damage if it is not addressed.
  • Information: An alarm to provide information. The system is operating normally.
NOTE: The severity is based on the system and does not necessary reflect the severity for the system application.

To view the message list in the display navigate to Protocol > All messages.

NOTE: User login with Service access level is needed to view the protocol page.

Message Name Severity Description
General
Urgent alarm Critical One or more urgent alarms are present.
Non-urgent alarm Warning One or more non urgent alarms are present.
Common alarm Critical One or more alarms that are configured for the common alarm are present.*
Operation Mode
Float charge Indication The rectifier float charge mode is active.
Charge (Boost charge) Indication The rectifier boost charge mode is active. The rectifier DC output voltage is higher than float charge voltage.
Equalizing charge Warning The rectifier equalizing charge mode is active. The rectifier DC output voltage is higher than float and boost charge voltage.
Direct feed Warning The rectifier direct feed mode is active. Battery might not be charged anymore.
Battery operation Warning The batteries are being discharged to supply the load.
Breaker Status
Mains circuit breaker open Critical The input breaker is open.
Battery circuit breaker open Critical The internal battery breaker and/or the external battery breaker is open.
Output mcb tripped Critical The output breaker is open.
Surge voltage prot. tripped Warning The AC input surge arrester has tripped.
Input breaker trip or off Critical One or more individual module input breakers has tripped.
Distribution fault Warning One or more outgoing feeders in the system or in an external distribution has tripped
Mains circuit breaker open* Critical The input breaker and/or the dual input breaker is open.
Rectifier Mains
Mains voltage out of range Warning The rectifier mains input is out of tolerance. Depending on the cause the modules might not run.
Mains error Warning The rectifier mains input is not available. The modules cannot operate.
Modules / Output
Module fault Warning/Critical* One or more modules are inoperable.
Fan fault Warning At least one of the fans is rotating too slowly or is inoperable.
Device temperature high Warning One or more rectifier modules are above the high  temperature level.
Converter overtemperature shutdown Critical One or more rectifier modules are above the temperature shutdown level.  The modules will run with reduced output power.
Output voltage out of range Critical The output voltage is above or below the tolerance level.
Converter overvoltage shutdown Critical One or more modules switched OFF because of too high output voltage.*
Output power warning Warning One or more rectifier modules have reached power limitation (modules are overloaded).
Current limiting Warning One or more rectifier modules have reached current limitation (modules are overloaded).
Battery
Earth fault plus circuit Warning Leakage current from the positive pole detected.
Earth fault minus circuit Warning Leakage current from the negative pole detected.
Battery current limitation active Indication The battery charging current has reached its maximum limit. The rectifier will regulate the DC output current to not overcharge the batteries with a too high charging current.
Battery test Indication The battery test is running.
Battery test error Critical The battery is discharged or weak. The battery is unable to supply the DC load in case of an AC failure.
Battery test not allowed Indication The conditions to start the battery test is not meet.
Battery circuit test failed Critical The battery is discharged, weak or not correctly connected. The battery is unable to supply the DC load in case of an AC failure.
Battery circuit test blocked Indication The conditions to start the battery circuit test is not meet.
Temperature sensor fault Warning No signal available from the temperature sensor.
Output voltage high Warning The system output voltage is above the set high voltage level.
DC voltage low Warning The DC  voltage is below the set low voltage level.
Battery exhaustive discharged Critical The battery is discharged. The connection between the battery and the load must be opened to avoid permanent damage to the battery.
Redundancy and Blocks
Current redundancy error Critical Only for redundant N+x and N+N module configurations. The redundancy is currently not available because of some inoperable modules. (Calculated based on output current).
Address redundancy error Critical Only for redundant N+x and N+N module configurations. The redundancy is currently not available because of some inoperable modules. (Calculated based on number of modules).
Address redundancy warning Warning Only for redundant N+x and N+N module configurations. The redundancy is currently reduced because of some inoperable modules. (Calculated based on number of modules).
Boost charging blocked Indication Boost charge mode is blocked. The mode can be blocked by an external/internal signal.
Equalize charging blocked Indication Equalizing charge mode is blocked. The mode can be blocked by an external/internal signal.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?