0000649744_02_en

Emergency Operation

If the communication between the controller and the modules is interrupted, the modules switch to emergency operation.

The parameters for emergency operation are pre-configured and cannot be changed. The set voltage level depends on the modules, for the value see the Technical Data.

Part Status
Rectifier mains Available and within the tolerance range.
Rectifier mains breaker Closed
Rectifier modules Running and suppling the load with the default voltage setting. Connection with controller is interrupted.
Battery Available
Battery breaker Closed
Output Available and within the tolerance range. The load is supplied.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?