0000649744_02_en

Module Configuration for N + 0, N + 1 and N + x

N + 0 Configuration

No redundancy of modules. The system has exactly as many modules installed as it needs to supply the full load and charge the battery.

N + 1 Configuration

One redundant module. The recommended and standard configuration. If one module becomes inoperable or needs to be replaced, the remaining modules can still supply the full load and charge the battery.

N + x Configuration

A specified number of redundant modules. In case additional redundancy is requested, x additional modules can be added. If x number of modules becomes inoperable, the remaining modules can still supply the full load and charge the battery.

Rectifier Module Configuration for N + 0, N + 1 and N + x

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?