0000649744_02_en

Module Configurations

Depending on the customer requirement it is possible to have different types of module configurations, with or without redundancy. The N + 0, N + 1 and N + x have the same configuration and use the same input source. For the 2N configuration two independent input sources are required.

NOTE: N stands for the number of modules required to supply the full load that the system is designed for.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?