0000649744_02_en

Default User Settings

CAUTION
unauthorized access
Always change your user settings (name and password) after the first login. Follow your site’s security protocols when selecting a new name and password.
After a full controller reset the system resets the user settings and it is necessary to change the user settings again.
Failure to follow these instructions can result in injury or equipment damage.

The system is delivered with the default user settings. Change the default user settings directly after the first login.

It is recommended to store the new passwords in a secure way so that they are not forgotten, for example by using a password manager.

Default User and Password Settings

Access Level Default Username Default Password
Viewer
Owner OWNER OWNER
Service SERVICE SERVICE
NOTE: A user is automatically logged out when the screen turns off. Default setting is after 3.5 minutes of inactivity, this can be changed under Settings > General > Display.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?