How to Change to Battery Operation
| NOTICE |
|---|
|
Battery DAMAGE
When the battery is at the end of discharge, the connection
between the battery and the load must be opened to avoid permanent
damage to the battery.
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
Loss of Output Voltage
After battery operation the battery is discharged it may
take several hours to recharge the battery. Recharge duration depends
on battery data and state of charge.
Failure to follow these instructions can result in equipment damage.
|
If battery operation is manually enabled the rectifier modules output is reduced to simulate that the rectifier mains is unavailable and to discharge the battery.
- Make sure you are logged in as a user with Service access.
- Press the Settings icon and navigate to Service > DC System 1 > Switching operations.
- Press the Battery operation button.
- Confirm the change.
The system has changed to battery operation. When battery operation is manually enabled the system will not automatically switch back to float charge.
When the battery voltage has reached the reduced voltage level of the rectifier modules, the rectifier modules will take over and supply the load, but the system will still indicate that it is in battery operation. The system needs to be manually switched back to float charge.