0000649744_02_en

Battery Tests

There are two types of battery tests. Both tests can be started manually and configured to automatically start at certain interval, if allowed to start.

The battery circuit test checks that the battery is connected and ready to supply the load if the rectifier output is reduced.

The battery test is a battery capacity test with a partial discharge of the battery. Different requirements for the test can be specified:

  • Discharge over a specific period of time.

  • Discharge with a specified capacity.

NOTE: It is possible to select if only one or both criteria must be meet for a successful battery test.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?