0000649744_02_en

2N Configuration with One of the Rectifier Mains Unavailable

If one of the rectifier mains becomes unavailable in a system with a 2N configuration, the other rectifier mains will still supply one group of modules. One group of modules is enough to supply the full load and charge the battery. The group of modules can be N, N+1, N+x or N+N.

Part Status
Rectifier mains 1 Available and within the tolerance range.
Rectifier mains 2 Unavailable / Unknown
Rectifier mains 1 breaker Closed
Rectifier mains 2 breaker Closed / Open
Rectifier modules Half of the modules connected to the rectifier mains that is still available are running and suppling the load. The other half is ready to operate when the unavailable rectifier mains return.
Battery Available / Charging
Battery breaker Closed
Output Available and within the tolerance range. The load is supplied.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?