0000649744_02_en

Additional Measurement Devices

As an option, additional measurement devices for certain voltages, currents and frequencies can be installed on the cabinet door. The additional measurement devices need to be specified when the system is ordered.

For details about any installed instruments refer to the Single Line Diagram and the Drawings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?