0000649744_02_en

Module Functionality

The compact power module contains all the internal components for the power supply or converter system. No other external power components are required or recommended, but some options exist to cover special requirements.

Multiple modules can be used in parallel to achieve different ratings and configurations. The modules are placed in racks inside the system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?