0000649744_02_en

Boost Charge

NOTICE
High output voltage
Before you change to boost charge mode:
  • Make sure the boost charge voltage level does not damage the load.
  • For critical or sensitive loads always check the boost charge settings.
  • If necessary, disconnect the load.
Failure to follow these instructions can result in equipment damage.

Boost charge mode charges the battery faster than float charge. Automatic boost charge can be used to define if and when the system should switch to boost charge automatically. It is also possible to manually switch to boost charge.

The rectifier modules supply the load and charge the battery but at a higher voltage. In case the mains input supply is unavailable, the battery will supply the load.

This mode is a temporary mode and is only used for a limited period.

NOTE: It is possible to inhibit boost charge mode. If boost charge mode is inhibited, the rectifier modules cannot automatically or manually change to boost charge mode. Boost charge mode can be inhibited permanently (not available for the system) or by an external signal.
Part Status
Rectifier mains Available and within the tolerance range.
Rectifier mains breaker Closed
Rectifier modules Supplying boost voltage to the battery and the load.
Battery Available / Charging
Battery breaker Closed
Output Available and the load is supplied if the load is approved for the higher voltage, else disconnected to protect the load.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?