0000649744_02_en

Equalizing Charge

NOTICE
High output voltage
Before you change to equalizing charge mode:
  • Make sure the equalizing charge voltage level does not damage the load.
  • For critical or sensitive loads always check the equalizing charge settings.
  • If necessary, disconnect the load.
Failure to follow these instructions can result in equipment damage.

Equalizing charge mode uses a high output voltage to overcharge the battery, to for example help remove sulfate crystals, as part of maintenance for the battery.

This mode is a temporary mode and is only used for a limited period.

NOTE: Equalizing charge can only be activated manually.
NOTE: It is possible to inhibit equalizing charge. If equalizing charge is inhibited, the rectifier modules cannot manually change to equalizing charge. Equalizing charge be inhibited permanently (not available for the system) or by an external signal.
Part Status
Rectifier mains Available and within the tolerance range.
Rectifier mains breaker Closed
Rectifier modules Running at a higher voltage setting to intentionally overcharge and condition the batteries.
Battery Charging at a higher volt.
Battery breaker Closed
Output Available and the load is supplied if the load is approved for the higher voltage, else disconnected to protect the load.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?