0000649744_02_en

Float Charge

Float charge mode is the standard operation mode for the rectifier modules. The output voltage depends on the float charge settings.

The rectifier modules supply the load and charge the battery. In case the mains input supply is unavailable, the battery supplies the load.

Part Status
Rectifier mains Available and within the tolerance range.
Rectifier mains breaker Closed
Rectifier modules Supplying float voltage to the battery and the load
Battery Available / Charging
Battery breaker Closed
Output Available and within the tolerance range. The load is supplied.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?