Battery Operation
| NOTICE |
|---|
|
Battery DAMAGE
When the battery is at the end of discharge, the connection
between the battery and the load must be opened to avoid permanent
damage to the battery.
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
Loss of Output Voltage
After battery operation the battery is discharged it may
take several hours to recharge the battery. Recharge duration depends
on battery data and state of charge.
Failure to follow these instructions can result in equipment damage.
|
In battery operation the battery is being discharged to supply the load. The system switches to battery operation in case the mains supply becomes unavailable. It is also possible to manually switch to battery operation.
| Part | Status |
|---|---|
| Rectifier mains | Unavailable and/or outside the tolerance range. |
| Rectifier mains breaker | Closed |
| Rectifier modules | Ready to operate when the mains return. |
| Battery | Discharging and supplying the load. |
| Battery breaker | Closed |
| Output | Available and within the tolerance range. The load is supplied by the battery. |