0000649744_02_en

Module Configuration for 2N (Dual Input)

For additional redundancy another input can be used to supply a second group of modules. Meaning that the number of modules needed to supply the nominal load is doubled. The modules are organized in two groups. With half of the total number of modules in each group. Each group is connected to an independent input source. One group of modules is enough to supply the full load and charge the battery.

It is possible to have both dual input and N+1, N+x, or N+N, for a total amount of modules equal to 2 * (N+x).

Rectifier Module Configuration for 2N (Dual Input)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?