0000649744_02_en

Modular System Functionality

The systems functionality depends on what type of modules are used and the configuration of the modules. For communication the NMC card is the default solution with other options available on request. Optional ADBUS card can be installed for additional inputs, outputs and features.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?