0000649744_02_en

How to Turn On the System

IMPORTANT: The modules will start to run as soon as the input supply is available. When the modules run the rectifier output will be energized. If the system does not have any output breakers or output feeders, the output terminal will also be energized as soon as the modules run.
NOTE: Read the complete procedure before you turn on the system.
  1. Check that all main breakers and module switches are open and that the load is disconnected.
  2. Close the rectifier mains breaker(s). The Display starts and after a few moments and shows the Home screen.
    NOTE: If active, turn of the audible buzzer by pressing the Mute icon in the upper right corner of the Display. The Mute icon is only visible if the audible buzzer is active.
    NOTE: If the Display has not started, check that the internal PSU switches are closed.
  3. If available, close all the rectifier module input switches.
  4. Check that all rectifier modules have started up. Check that the green LED is illuminated on all rectifier modules, and that no red LED is illuminated or flashing.
  5. From the Home screen click on the Rectifier modules icon. Check that the rectifier output voltage is according to the float voltage on the Data sheet.
  6. Close the battery breaker(s).
  7. Press the Double arrow icon and check that no alarms are active, except for any open output breaker or output feeders.
  8. If available, close the output breaker(s) and any output feeders.
  9. If needed, reset any held alarms. Press the Double arrow icon and then press the Reset held alarms button.
  10. Check that the system runs correctly and that no alarms are active.
The system is ready to supply the load.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?